REC.TRIGSLOPE
Description
REC.TRIGSLOPE sets the recorder trigger slope. This parameter is not used when REC.TRIGTYPE is 0 or 1.
Value | Description |
---|---|
0 | Negative |
1 | Positive |
Examples
Code
Trigger the capture on a positive rate of change.
-->REC.TRIGSLOPE 1
Context
For more information see Scope.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 1 |
Default Value |
1 |
Data Type |
Integer |
See Also |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.